Vajate rohkem?
Kogus | |
---|---|
1+ | 100,810 € |
Tooteteave
Toote ülevaade
The LIVESCAN ANTENNA KIT from Siretta is an antenna kit for directional liveSCAN 3G GSM surveys with the SNYPER-3G spectrum. The SNYPER liveSCAN antenna kit is an accessory to be used with the SNYPER-3G Spectrum signal analyser to establish maximum GSM signal strength direction. Using liveSCAN produces a live, real time graph on the SNYPER display showing strength level with direction of the handheld antenna. The antenna held in one hand and the SNYPER in the other and turing thru 360˚ the operator can see visually from the real time graph being drawn on the SNYPER display which direction the maximum signal is. This process can also be used to determine in which direction the largest GSM signal of all the networks in the area is coming or the direction of the maximum signal strength of a particular network as desired.
- Enables Live scanning for max signal strength when used with the SNYPER-3G spectrum
- Gives real time chart of 3G signal strength v. direction of antenna
- Can 'lock' to a network and establish max signal direction
- 1.5M of antenna cable to connect to SNYPER-3G spectrum
- Comes with a 2G/3G yagi directional antenna with a convenient user handle
- Comes with 1.5M of RG58 extension cable to connect to the SNYPER-3G Spectrum
Rakendused
Test & Measurement, Signal Processing
Sisukord
LIVESCAN ANTENNA KIT, Rugged carrying box, Instruction guide.
Tehnilised andmed
GPRS, 2G/3G Yagi Antenna, 1.5M RG58 Extension Antenna Cable, Hard Carrying Case
No SVHC (21-Jan-2025)
-
Tehnilised dokumendid (2)
Seadusandlus ja keskkonnateave
Riik, kus toimus viimane oluline tootmisprotsessPäritoluriik:Romania
Riik, kus toimus viimane oluline tootmisprotsess
RoHS
RoHS
Toote vastavussertifikaat